Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hi all,I'm developing a bipolar stepper motor application by means of a STEVAL-PCC009V2 + EVAL6480H boards coupled together.My application have to follow a position by means of an incremental encoder that is connected to the encoder quadrature module...
Posted on December 18, 2014 at 17:57Hi,does anyone know when the EVAL6480H-DISC will be available in the UK? Also will it be cheaper than the EVAL6480H evaluation board?Thanks in advance,Howard Smith #eval6480h #eval6480h-disc #l6480
Hi at everyone,I designed a open loop dc/ac converter, but I met a big problem. The high side output did'nt work correctly over the 40V of Vhv. Over that value the output goes out derivates and the resistance from pin 14 and pin 13 is 5ohm. Aflter a ...
Hi!I design a board on which there will be several microcontrollers (STM32 and ATMEGA328), 12V comes on the board and I need to lower this voltage to 5V. In addition to the controllers, I will power a few more sensors and LEDs.I am trying to find a r...
Hi, I'm trying to build a power meter that has the ability to switch on and off the attached load.The power supply for the design is created using Viper26LD in buck mode, the processor used to control the design is STM32L051. The entire design analog...
Hi, I have questions about how serial DC-DC converters work for photovoltaic systems. For, the current in the output tends to be different due to MPPT, which would be several sources of current in series. I read the manual that explains the SPV1020, ...
Could you please let me know, which land pattern do we need to consider for PowerFLAT 3.3 x 3.3 package,for STL6P3LLH6? Whether we need to consider Type C or Type F package? The data sheet doesn't clearly say which is defined by what and neither do...