Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nmos transistor problem

Good morning; I want to do a simple relay controlled by my nucleo board; so I did a simple circuit with the STP55NF06L; however, it does not work as expeted, in real ife, even when I am not sending voltage to the gate, the transistor conducts electri...

Capture d’écran 2025-07-17 à 08.08.17.png Capture d’écran 2025-07-17 à 08.09.07.png
Jad by Senior
  • 543 Views
  • 1 replies
  • 0 kudos

STUSB4710 on a 3 port USB hub

Hello,I want to use 3x mentioned devices in a usb hub to deliver pover to peripherals.Does anyone has experience with something like this? Can it negotiate with three different devices or it will cuse some trouble.? Best regards, Mrdjoni  

miroslav by Associate III
  • 326 Views
  • 0 replies
  • 0 kudos

Viper35 waking up issue.

Hello,For the past few days, I’ve been trying to operate the VIPer35 quasi-resonant  offline high-voltage converter, but I haven't been able to get any output. I attempted to bypass or disconnect the output of the PC817 optocoupler and also tried sho...

ST1PS02D1QTR VOUT2 Output Discharge

I have ST1PS02D1QTR (output discharge disabled variant). However, I am observing that if AUX = low but external 1.2V is applied to VOUT2, I get power dissipation that seems in-line with output discharge resistance on VOUT2. My question is this: does ...

jmjec by Associate
  • 249 Views
  • 0 replies
  • 0 kudos

L4931 Output Capacitor

A design I am debugging is utilizing Y5V dielectric capacitors on the input and output of the L4931. There is a 2.2uF capacitor directly at the output and another 2.2uF capacitor on the other side of an ~4 Ohm resistor that analog supplies are used o...

ETarver by Associate
  • 472 Views
  • 1 replies
  • 0 kudos

STEF01 Output Clamp 32V Max?

I have recently designed the STEF01FTR into a design that sits on the main input rail. The input is specified to run from 9V-48V. As a result the output VClamp is set the 52V max by setting R122 to 560K and R126 to 10K. When our initial FAI boards ar...

STCS1A

Hi I am using STCS1APUR to drive 10LEDS IR, (MTSM5116MT2-BK), circuit belowcurrent should be 1A as of f/b resistance, enable gets turn on as sson as the STM32 MCU comes up, supplying a 3.3VDC PWM though the MCUissue:the voltage drop across the led is...

nmohammad_0-1752242913431.png

Resolved! VIPER31 switching losses

Hi,I would like to use the VIPER319HDTR and would like to check the thermal to see if Tj will be an acceptable value.However, the switching losses of the internal FET are not mentioned. Is the switching time of the internal FET known? Or is there ano...