Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I can get my L9960T Evaluation board to work!

I am currently working on a project where we would like to use the L9960T and therefore we have ordered a EVAL-L9960T board.We need to use it only as a simple H-bridge without benefiting from the SPI settings and diagnostics capabilties.I have now be...

CHans by Associate
  • 582 Views
  • 0 replies
  • 0 kudos

Designing doubts with SPV1040

I need to charge LiPo battery with solar cell. I found out the SPV1040. But the datasheet doesn't provide enough details, I was unable to find any document to help me, and the eDesignSuite doesn't work. Related documents use it with L6924. Can I simp...

HBalt by Associate
  • 641 Views
  • 0 replies
  • 0 kudos

Resolved! STEF01 output voltage too low

Our customer is using STEF01 e-fuse in a system with 24V input at VCC. See schematic below. Without any load in parallel to C25 they get around 23V at the output. But as soon as they put any charge (e.g. 10Kohm resistor) at VOUT, output voltage goes ...

0690X00000ARJuTQAX.png

STM32F103 power management

Hello,I m designing a board with a STM32F103. I was wondering about capacitors value. In STM32 documentation, it's written to use 100nf per VDD PIN + one 4.7uF. On the other side, I m using a low dropout regulator :I dont' understand where to place ...

0690X00000ARJmeQAH.png 0690X00000ARJnXQAX.png
BAure by Associate II
  • 984 Views
  • 0 replies
  • 0 kudos

Layout Recommendation for inverting DC-DC Converter MC34063

I am using the MC34063ECD-TR to take 5V and make -12V. I'm using the schematic as recommended in the datasheet for this application (with the exception of using a 100uH inductor instead of a 90uH inductor). It is working nicely electrically - I get...

MHolt.16 by Associate II
  • 4297 Views
  • 5 replies
  • 0 kudos

Can STEVAL_POE002V1 work as 24V source?

I bought the STEVAL_POE002v1. It works fine at 5 V. Now I want to setup a POE with 24V. Can I achieve this with that STEVAL? I would think to change the transformer and to adjust the Feedback-path and perhaps the Fsw. Can you help me with a calculati...

WEmme by Associate II
  • 1162 Views
  • 1 replies
  • 0 kudos

STM6600 VCCLO

The description of the VCCLO pin says it goes low when Vcc is below Vth+.However, the timing diagrams 20 and 21 show VCCLO going low tdebounce after VCC drops below Vth-.Which is correct?

Acoustic Noise L6599

I absolutely do not understand under what conditions and for what reason sometimes during operation of the LLC converter, the power transformer emits audible high-frequency acoustic noise. Some instances work fine, but some make a good audible noise....

IStel by Associate
  • 1545 Views
  • 2 replies
  • 0 kudos
yqn by Associate
  • 693 Views
  • 0 replies
  • 0 kudos