Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 for ACIM

I want to develop ACIM drive with power output upto 1KW. What STM32 series processor will be suitable? I would like to have good firmware support for development.

NKale by Associate II
  • 761 Views
  • 0 replies
  • 0 kudos

Resolved! How to sync multiple L7987 DC/DC Switching Converters

We are planning to use three L7987 DC/DC switching regulators on our interface module. All L7987 should be synchronized and should operate with the same frequency set with an external resistor on the pin FSW.In datasheet https://www.st.com/resource/e...

0690X000009jJkTQAU.jpg

Can I use HVLED001A with a resistive load up to 250W;

Can I use HVLED001A with a resistive load up to 250W;The load is up to 6A or 9A, 20V to 28V and must be below 50V. The waveform could have a a lot of rectified mains ripple because it is a simple steel wire heating element so I am considering using m...

why do I see unexpected behavior with Steval-ihm023v3?

Hello,I am using the driver Steval-ihm023v3 to run a PMSM. Previously, I used one of the TI low voltage drivers and ran my motor. Now I am using the low voltage configuration of the Steval-ihm023v3, namely "35V only", but I see weird behavior when I...

AKhia by Associate
  • 650 Views
  • 0 replies
  • 0 kudos

Steval-esc001v1 over-current protection(OCP)

I bought a Steval-esc001v1 board and use the FW built in version 5.4.1. Everytime i boot the board,it always showed the over-current flag.Even i don't connect the motor,change HW or FW. The program exactly triggered the TIM1 BRK2 interrupt.But i foun...

Hw by Associate
  • 616 Views
  • 0 replies
  • 0 kudos

Battery Analyzer for Electric vehicles

Dear Sir/Madam,We want to design a Battery Analyzer for Electric Vehicles such as Plugin Hybrid car(PHEV), EV passenger car,Heavy delivery van.The battery voltage can be the range of 9 VDC to 800 VDC. Please suggest us a appropriate part or design wh...

AKUMA.62 by Associate
  • 878 Views
  • 1 replies
  • 0 kudos