cancel
Showing results for 
Search instead for 
Did you mean: 

STEF01 output voltage too low

Central SUPPORT
Senior II

Our customer is using STEF01 e-fuse in a system with 24V input at VCC. See schematic below. Without any load in parallel to C25 they get around 23V at the output. But as soon as they put any charge (e.g. 10Kohm resistor) at VOUT, output voltage goes down to lower than 2V (!).

Customer has tried several different configurations of the STEF01, but did not figure out what is causing the problem.

0690X00000ARJuTQAX.png

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Central SUPPORT
Senior II

In interaction with customer we also checked the PCB layout and finally identified the root cause: the “exposed pad�? was not connected. In fact, the exposed pad is internally connected to the power element drain and essential to proper power and thermal dissipation of the device.

Therefore it is absolutely mandatory to connect the input pins and exposed pad of the STEF01, see datasheet.

0690X00000ARJvvQAH.png

0690X00000ARJw0QAH.png

View solution in original post

1 REPLY 1
Central SUPPORT
Senior II

In interaction with customer we also checked the PCB layout and finally identified the root cause: the “exposed pad�? was not connected. In fact, the exposed pad is internally connected to the power element drain and essential to proper power and thermal dissipation of the device.

Therefore it is absolutely mandatory to connect the input pins and exposed pad of the STEF01, see datasheet.

0690X00000ARJvvQAH.png

0690X00000ARJw0QAH.png