Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

powerSTEP01 package (VFQFPN 11x14x1.0 mm) thermal resistance

For documentation purposes i need to estimate the worst case temperature for the powerSTEP01 that occurs in our application. I already calculated the worst case power dissipation so i am able to determine the temperature with information about the "j...

RSopp.1 by Associate
  • 534 Views
  • 0 replies
  • 0 kudos

STM32G071 Can't read ADC Measurements through IN15

Hello CommunityRecently I'm in a project with the NUCLEO-G071RB.I been working with ST boards for a long time but this time, i cant make measurements through specific channel "ADC_IN15". Pin PB11I made other channels to work ( IN0, IN1 etc...) but w...

CAvil.1 by Associate II
  • 901 Views
  • 1 replies
  • 0 kudos

STC3117 Fuel Gauge not entering CC mode when discharging, but does enter CC mode when charging. Why would the fuel gauge work for charging, but not for discharging?

Hello,I have a custom board with a STC3117 as the fuel gauge to a 5200mAh lithium ion battery pack. The pack can charge up to 1.5A and discharge to up to 3 A. The issue I am seeing is that the SOC will be stable with the system running. When I charge...

TTIED.1 by Associate
  • 777 Views
  • 0 replies
  • 0 kudos

STEVAL-IHM023V3 in "3-phase HV FOC control for SMPMSM". We plan to use external control with 5V digital signals for all inputs (E-stop, PWM-H,L, brake, etc), It is save to set the Vdd at 5V in that case?

We're planning to develop some motor drive academic boards for SMPMSM FOC motors for Master Students and for one of the parts we're using is STEVAL-IHM023V3. We're currently development the platform.In the manual UM1823, page 28, table 6 for FOC cont...

CC.1 by Associate
  • 564 Views
  • 0 replies
  • 0 kudos