User Activity

HelloI have ATEAVAL-IPFC01P1 and I have two questions during the test of operation.If the load is not applied, it operates normally,however, PWM1 and PWM2 signals are not output when load is applied.As a result of checking the signals of STEVAL-IPFC0...
Helo,I have recently bought a STEVAL-IPFC01P1, to evaluate de STNRGPF01 controller.I want input voltage spec to 90-265VAC at 47-63Hz rangeHow can I change it?I'm tried the following way...1) Interleaved PFC Specifications clock2) "Mains Wide Range Li...
Helo,I have recently bought a STEVAL-IPFC01P1, to evaluate de STNRGPF01 controller.I want input voltage spec to 90-265VAC at 47-63Hz rangeHow can I change it?I'm tried the following way... 1) Interleaved PFC Specifications clock 2) "Mains Wide Range ...