User Activity

High-Side Switch VN9004AJTR is fairly new, so nothing on the web to help with circuit and program design. It has a simple default circuit and MCU programming configuration, but it has some nice features that require more complex programming. Has any...
Compile error is: make[1]: *** No rule to make target 'C:/Users/david/STM32CubeIDE/workspace_1.1.0/SPIN3201/SDK5x - STEVAL-SPIN3201 - BullRunning/Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_exti.c', needed by 'Drivers/STM32F0xx_HAL_Driver/stm32f0x...
We generate the firmware code using the Motor Control Workbench that calls the STMCubeMX that then calls the STMCubeIDE. We were able to successfully compile the firmware this way using the IAR IDE, but we get many compiler errors with the STMCubeIDE...
This 5-Part course on BLDC Motor Control: https://blog.st.com/motor-control-mooc/?ecmp=tt12026_gl_enews_jul2019&cid=stmDM20193&bid=233348316&uid=s6xclNpic16UkdrZURLncBqshV3hp5u8 discusses a "Motor Parameter Calculator" Excel spreadsheet at minute 7 o...
Also, there are many source code modules provided in the software download, but there doesn't seem to be any explanation of which modules to compile to run the BLDC controller.
Kudos from