Skip to main content
Rsi
Associate II
July 11, 2019
Question

Can stm32 control the VNQ5160?

  • July 11, 2019
  • 0 replies
  • 458 views

Hi. I have some questions.

I want to use stm32 to control vnq5160 with 12Vdc system.

My friend designed the circuit with stm32 and vnq5160 and artwork too.

after soldering, this board works well.

And another person artwork with same circuit, and I soldered, but this board doesn't work.

The output is always on High(12Vdc). If I remove the resistor of STAT_DIS, the output is always LOW(0Vdc).

The difference between first one and my one is size of chip resistor, and the resistor value connect to gnd pin.

First one use zero ohm, and I use too, but doesn't work.

I've changed the resistor value but doesn't work.

please help me and thank you for reading.

  • designed circuit

  • my one

  • first one

This topic has been closed for replies.