STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
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
VNijh
Associate
since
2019-07-06
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About VNijh
Options
Report User
User Activity
Posts
Replies
I would request a DC Load design for testing 15 batteries in series at 20 amps of current. I would like to use an igbt with sg3525 at 20 kHz. Regards
2020-03-22
Hello community, Question is related to application note no. 308
2019-07-10
Please help to use two anti-parallel SCRs in place of a single triac ? Regards and thanks in advance.
Dear Sir/Madam, My question is related to your application note no. 308
2019-07-06
I wish to use two anti-parallel SCRs for controlling a transformer with specifications of Pri:220V, Sec:7V, at 3500 amps. Is it possible ? What changes , if any, are required in the circuit ? Please help.Regards.
Dear Sir/Madam, My question is related to your application note no.308.
2019-07-06
No replies to display.