User Activity

Hi, I'd like to run the bldc with (NUCLEO-F746ZG + IHM07M1), so I tried to use 'ST Motor Profiler', but the program said that 'control board communication still missing'.​I did remove the Solder bridges and powered 12V on power board, connected the U...
Hi. I have some questions.I want to use stm32 to control vnq5160 with 12Vdc system.​My friend designed the circuit with stm32 and vnq5160 and artwork too.​after soldering, this board works well.​And another person artwork with same circuit, and I sol...
Hi. I designed the power conversion circuit with A6986.​After soldering of this pcb, I powered 24V on power line.​And the VIN pin(#15) was damaged.​I have no idea what is the problem.​when I design the circuit, I consulted the manual, and eval. board...
Hi. I'm trying to control bldc using esc001v1, but I cannot connact to motor control workbench.And motor profiler doen't works too.When I using motor profiler, it tells me that f/w doesn't match and after upgrade the f/w, it telling me that serial po...
Kudos from