Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! L6474 : behaviour of status register

Hi, starting from the documentation :"The UVLO, TH_WRN, TH_SD, OCD, NOTPERF_CMD and WRONG_CMD flags are latched: when the respective conditions make them active (low or high), they remain in that state until a GetStatus command is sent to the IC. "My...

JulienD by Senior
  • 853 Views
  • 2 replies
  • 0 kudos

Resolved! The leakage current of L6470H's ADCIN pin

Please see the attached picture. Our company is using L6470H chip for our design. According to the typical application in the datasheet, we want get 3V on the ADCIN pin. Our Vs is 24V and the voltage divider resistors that we chose are Ra= 13K and Rb...

MSui.1 by Associate
  • 1912 Views
  • 3 replies
  • 0 kudos

Resolved! How can I incorporate X-CUBE-SPN5 into STFM32CUBEIDE

I have downloaded a copy of the en.x-cube-spn5 but I am unsure how to add this to the STM32CUBEIDE to allow me to run the example programs. I would then like to develop new applications using a pair of X-NUCLEO-IHM05A1 boards and a Nucleo-F401RE boar...

JWhit.3 by Associate II
  • 1168 Views
  • 2 replies
  • 0 kudos

Resolved! External diode in L6390 for high switching frequency

Hello. I have a custom made board with an L6390 used to drive two MOSFETs. My switching frequency is 100kHz. I noticed that at low duty cycles the bootstrap capacitor was not charging correctly. Per the datasheet, I discovered that due to the interna...

CGonz.2 by Associate
  • 1591 Views
  • 3 replies
  • 0 kudos