Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BTA41-600BRG Related certificates

We are a factory for new energy vehicles. I would like to find a CCC or CQC or CE certificate for this model.  Could you please provide us with it? Thank you!

KCAO.1 by Associate
  • 674 Views
  • 1 replies
  • 0 kudos

LED6000 understand the Bandwidth in eDesign.

Building a very big LED array and need to get the frequency of the LED6000 up to about 1MHZ. But working with eDesign I find that a bandwidth error comes up a lot. When I hover over it to more information it show something about TON. Trying to nar...

0693W000004JH9dQAG.png
JZigr.1 by Associate
  • 576 Views
  • 0 replies
  • 0 kudos

Resolved! What is the definition of tick time?

I am developing the firmware to control the L6470 IC.On my board the L6470 uses an internal clock.The main factor in motor control is tick.There is no information on tick setting in the L6470 data sheet, all calculations are based on 250ns.When using...

scho.1 by Associate
  • 1236 Views
  • 1 replies
  • 0 kudos

Resolved! What is the L6474 ABS_POS register really reporting?

I am looking at using the L6474 to drive a stepper motor. I have a question about the absolute position register (ABS_POS).It says it is the current motor absolute position, but I want to clarify that it really is just a counter for the number of ste...

DSabo by Associate III
  • 1038 Views
  • 2 replies
  • 0 kudos

X-Nucleo-IHM02A1 & STM32 Nucleo F302R8 error code

Bonjour, je suis en train de travailler sur un projet dans lequelle je dois commander deux moteurs pas à pas, j'ai acheté le driver IHM02A1 et la carte Nucleo-F302R8 .j'ai suivi toutes les étapes disponibles dans le guide de démarrage disponible par ...

k.B.8 by Associate
  • 819 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.