Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Automatic radiator control valves

Hi there,I am interested in automatic radiator control valves (energy harvesting or batteries powered). Do you have any suggestions?Thank you!Best regards,Oskaras

OAlša.1 by Associate
  • 599 Views
  • 0 replies
  • 0 kudos

SOF-IRQ when cascading 3 devices of LED1202

Hi, what is the behaviour of the IRQ-Lines of the LED1202 when connected wired-OR as in chapter 6.2 of datasheet (i.e. clock synchronized 1x Master, 2x Slaves)? I want to use SHFT=1 on all 3 devices.As per datasheet, the update of the PWM - registers...

Gera.V by Associate II
  • 815 Views
  • 0 replies
  • 0 kudos

Resolved! How to configure POWERSTEP01 ocd_th and stall_th?

I've set up the POWERSTEP01 driver in voltage mode, which works nicely. Now I want to use the sensor less stall detection feature to implement sensor less homing. How must the stall_th and also the ocd_th values be dimensioned for this to work correc...

ARöss.1 by Associate II
  • 6312 Views
  • 15 replies
  • 0 kudos

Resolved! STEF01 - what is the equivalent circuit of the ENABLE/FAULT pin ?

The ENABLE/FAULT pin delivers back a voltage that provides the part status (Table 6 of the DS).It is said that OK = 5V; thermal fault = 1.4V; power protection = 0V.As this pin must be directly connected to a 3.3V FPGA pin, I made some measurements wi...

AFARI.1 by Associate
  • 1091 Views
  • 2 replies
  • 0 kudos

Resolved! Schematic x-nucleo-ihm08m1 does not seem to the latest

Hello,I have the x-nucleo-ihm08m1 board and looking into the schematic I do not see the potentiometer R42 in there.I bought my board recently from mouser.The schematic i downloaded from the web page of the board (attached).Thanks in advance.

Hos by Associate II
  • 2208 Views
  • 2 replies
  • 0 kudos