Skip to main content
MHeue.1
Visitor II
May 11, 2020
Question

Has anyone experience with current limiting of motor drive VNH7100 and L9960 with stm32L433?

  • May 11, 2020
  • 0 replies
  • 451 views

Hello, I am using the stm32L433Rc and a maxon motor (9 V, initial current 11,4 A, continous current 3 A). Now I am looking for a motor drive inbetween. I am thinking of using the a) VNH7100 or b) the L9960. Has any one experience with one of these? I am worried about burning the motor with a) as I cannot limit the current here and with b) that the maximum provided current could be not enough for get the motor going.

Also I am wondering whether the VNH7100 is compatible with the stm32L433RC regarding the current sense function.

Thanks for your help!!!

This topic has been closed for replies.