Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STDRIVE101 or EVAL-L9907

My objective is to develop a sensored BLDC control.Right now I am collecting information and I find myself in the following situation.The motor has the following characteristics: V = 48 / 52VDC i I = 15 / 20A.I have seen the following STDRIVE101i eva...

JD.1720 by Associate II
  • 1493 Views
  • 1 replies
  • 0 kudos

How to use temperature compensation typical curves in STPM32?

How to know what curve do I need? In what cases do I need temperature compensation? Datasheet says "Reference voltage generators with programmable independent temperature compensation". What does word "independent" mean? Datasheet says only that:

0693W00000Bb1WzQAJ.png 0693W00000Bb1XxQAJ.png
KStuk.1 by Associate
  • 858 Views
  • 0 replies
  • 0 kudos

L6472 current consumption way higher than set current

Hello,I am using an L6472 stepper motor controller.I have an EVAL6472H board coupled over SPI to a nucleo L4R5Zi board on SPI.I am running the motor controller on Step Clock mode. I am setting the hold current to 200mA. When the motor runs, I am upda...

deshmukh by Associate
  • 842 Views
  • 1 replies
  • 0 kudos

How to control stusb1602 using stm32f103

I wanna to implement USBPD with stusb1602 and stm32f103.have 3 USBPD Port and implement control and operation with stm32f103.but i could not find any related information. According to document, that need to use stm32f072 to implement USBPD. ans so is...

MLee.14 by Associate
  • 2481 Views
  • 3 replies
  • 0 kudos

Resolved! Implement s-ramp on stepper

Hi, I need to implement an s-ramp for a stepper motor.Currently using L6482.Can you please point me in the direction of the correct controller + driver? Thanks!Uri

UDanz.1 by Associate II
  • 1975 Views
  • 2 replies
  • 0 kudos