cancel
Showing results for 
Search instead for 
Did you mean: 

Current sensing and SOC using STC3115AUT

ELin.3
Associate

Hi, there

On page 10 of the datasheet, it is recommended to use 5 to 0.05 ohm resistor for the current sense resistor connected between the CG pin and the GND. If the CG pin is connected directly to the GND, or BAT-, what does it mean to the current sensing and the accuracy of SOC ?

I was able to use the Power Saving Voltage Mode (VMODE = 1) to get a good reading of the battery voltage. Yet, I was hoping that I can use the SOC to better increase the accuracy of the FG reading. Unfortunately, no matter what I do, the SOC reading is never close to correct. Before I post the detailed register configurations, I want to know if the SOC or current sensing is even possible when the CG pin is connected to the BAT- directly.

Thank you for your time.

Regards,

Eric

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

A current sensor is required to measure the current. The STC3115 uses a shunt resistor connected between CG and GND.

If you connect CG directly to GND, no current measurement will be possible.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.