Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Ihm08m1 change shunt

hi I have the ihm08m1 how can I change from 1 shunt to 3 shunt if by default it is soldered on 1 shunt?

SDall by Associate II
  • 2240 Views
  • 4 replies
  • 0 kudos

L6480 UVLO-Bit problem. Can't get it flip to 1.

Hello,I use the EVAL6480 Board and the STM32 F446RE as MCU to communicate to the driver.My Steppermotor [1] (not exactly this but very similar) has oer phase a resistance of 1,2 ohm.My Problem is that the motor does not turn because the UVLO flag is ...

_legacyfs_online_stmicro_images_0693W00000FDGk6.png
Evdsl.1 by Associate II
  • 3019 Views
  • 5 replies
  • 0 kudos

UVLO flag always on

Hi, Using IHM03A1, I'm driving a 48V-9A motor.According to @Cristiana SCARAMEL (Employee)​ recommandations, I add 15mOhm/3W resistances in parallel of R1 and R2, so R1 and R2 value is now 13mOhm, I choosed current mode, set run current to 10.2A (132....

BL1 by Associate II
  • 2461 Views
  • 4 replies
  • 0 kudos

Resolved! POWERSTEP01. Is there a way to switch cleanly between MOVE and RUN?

3 Powersteps -> 3 steppingmotors for X, Y and Z axes, voltage mode.Is there a way to switch cleanly between MOVE and RUN commands?Currently, when I execute RUN command after MOVE movement, motors move too slowly. Although I change the speed (target -...

GoA by Associate
  • 1616 Views
  • 2 replies
  • 0 kudos

STPMIC1 I2C program

I have a STPMIC1E on my board, it is used with a STM32MP157 chip. I am currently trying to program the PMIC IC via the GUI but it won't connect to the bus. It says USB to I2C bus not connected. Any ideas?Thanks

Na.11 by Associate II
  • 1951 Views
  • 2 replies
  • 0 kudos