User Activity

The VIP ER06XS is up to 800V.The T1 is need to endure 600V.The D28 STTH1L06A is up to 600V.The STGD6M65DF2 IGBTs power stage featuring:– V(BR)CES = 650 VThe STSPIN32F0601 is up to 600V.
There are two ways of BLDC motor solution. The one of solutions is EVSPIN32F0601S3 and the other is EVSPIN32F0601S1. I want to drive BLDC motor with sensor less. Which solution is match the goal? The motor specification is 100V D.C. 1A 100W.