Resolved! Is the thermal pad of the L5150BNTR electrically connected internally to Pin 2 of the SOT-223 package?
I know I could take a meter and simply check but I don't have any spare parts easily accessible to make this quick measurement.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I know I could take a meter and simply check but I don't have any spare parts easily accessible to make this quick measurement.
VNH7040AYTR, does the part marking with any relationship on the tracecode of the label
I am having trouble finding a way to change the PDO’s listed in usbpd_pdo_defs.h. After manually changing the USBPD_PDP_SRC_IN_WATTS from 15 to 100, PORT0_NB_SOURCEPDO from 1 to 5, & also defined the PORT0_PDO_ListSRC, I still get the same results wh...
hello,I do have a question about the INT1 pin behaviour of the STPM32.I measured all pins with a saleae logic pro 16 and decoded the spi communication also.From the beginning, the initialization routine looks as described in the datasheet.It is at le...
I am designing a power metering circuit using the STPM34 IC, and I need to measure three channels of current. The STPM34 datasheet specifies that the device has two current measurement channels (IP and IN) and two voltage measurement channels (VIP an...
For a project using several powerStep01 drivers it would be very useful, if each powerStep01 could be identified by a unique ID or a serial number. In the interface description no such register is defined. Is there maybe a hidden register available w...
the reason is that I need to have it operating with 4.2v which seems not to be compatible out of the box
hi When confirming the footprint of STSPIN32G4(VFQFPN 9X9X1.0 64 PITCH 0.50), we find that the length of STSPIN32G4 =4.10+2.03*2+0.85*2=9.86(STSPIN32G4 - High performance 3-phase motor controller with embedded STM32G4 MCU - �?法�?�导体STMicroelectronics...