Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
关于交直�?混补设计,我的想法是会�?�时使用直�?和交�?:例如控制器�?�时接入太阳能�?�供电和交�?,在太阳能输入�?低时,输出功率下�?时,交�?�?�与工作用�?�弥补直�?因供电�?足缺少的那部分功率,我看�?的这样产�?有使用一个交错�?PFC,电机驱动是�?�一家的,想询问有关于交直�?混补设计的�?�考设计或者文档�?�
Hi I would like to know what is the total data acquisition time of converting all 12 cell voltages and pack current and when it will be available to access from communication bus. I was referring the datasheet, but the total data conversion acquisiti...
Hi, I hope this message finds you well. I have a query regarding the STPMxx energy metering IC and its Graphical User Interface (GUI). Specifically, I would like to know if it is possible to connect the STPM3x evaluation software directly to our micr...
I've tried two different boards: one is a custom PCB that should never draw more than 8 - 10 mA and another is a Teensy 3.2 with a Blink example loaded onto it.In both cases the LPM01A either fails to provide a high enough voltage (for the custom PCB...
I am currently experiencing some confusion regarding the graphical user interface (GUI) software for STPMS2 and STPM34 integrated circuits (ICs). While STSW-STPM005 appears to be exclusively designed for use with the EVAL3PHISO kit and the STPMS2 IC ...
Hello expert,I'm currently designing the power source board with STUSB4710AQTR, and have 2 questions.1: how does the protection function such as UVLO work? In case of the event, the IC enters the error recovery state according to the datasheet, but I...
I am looking to build a Power Supply that will vary between 2VDC and 15VDC in a Forward Converter Configuration. I need to produce an output of 200A. I have been advised by other engineers that I need to build a Parallel Configuration. I need a bit o...
I'd like to know STSPIN32G4 FIT Value to calculate MTTFdto meet SCF Level How can I find STSPING32G4 FIT Value?plesas let me know