Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Battery charger solution

Hi ST experts,Would like to know if ST has any recommendation on battery charging solution?The battery pack requirement is 7.4V 2300mAH which is 2-cells construction.The intention is to change from standalone battery charger IC to a smart charger sol...

STLearner by Associate III
  • 1087 Views
  • 1 replies
  • 0 kudos

Resolved! L6230Q excluded from longevity program?

We are using the L6230Q motor driver and on the main L6230 product page the 10 year longevity program is highlighted.However, on the longevity program list only the L6230 (PowerSO package) is listed, the L6230Q (QFN package) is not.The confusing part...

GaryA by Associate II
  • 2570 Views
  • 2 replies
  • 0 kudos

How to measure power consumption using STM32F767zi

Hello, I'm working on an STM32F767zi board and want to monitor the power consumption of the MCU using the X-NUCLEOLPM01A. I follow the instructions in the board's documentation to turn off the SB112, which is turned on by default. Can somebody tell m...

Aqsa by Associate II
  • 2044 Views
  • 3 replies
  • 0 kudos

STPM32 Datasheet update 2022

In the current version of datasheet, in the revision history there is written than on 23rd May 2022 there was update of Table 14. However I cannot see difference between Table 14 in the current datasheet and the datasheet I saved before (Rev8). Probl...

jeantil88 by Associate II
  • 1102 Views
  • 0 replies
  • 0 kudos

STEVAL-EFUSE01 Not working

Recieved a STEVAL-EFUSE01 for evulation of the STEF01 however I can not get any current to pass through it. 12v input on VCC and GND, a 1amp load on VOUT_F, Enable pin is floating, 22ohm resistor for current limiter should allow at more than a 1amp l...

TH3221 by Associate III
  • 2698 Views
  • 6 replies
  • 0 kudos

e-fuse evaluation board question

Hello. I have a STEVAL-EFUSE01 board that uses the STEF01 e-fuse at its heart. I take it out of the package. I connect 24V to VCC_F (supply). I don't connect anything to the VOUT_F output. What voltage should I read on that output?I think I should re...

RAlve.3 by Associate II
  • 1314 Views
  • 1 replies
  • 0 kudos