Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Suggestions to me use a 6V panel with SPV1040

Hi Team,I am looking to use a solar panel which gives 6v and I want to use the spv1040 mppt converter.What would you recommend I use with spv1040 as it has a max input of 5.5v. Is using a buck converter before the SPV1040 recommended?Regards,Nilav 

Couldn't configure IDs of L9963e-MCU Eval KIT

hello. I operated the EV KIT with the STSW-L9963E GUI, and checked until the MCU was connected. After that press the "Configure IDs" button and the ACK LED will change from green to red. And then there is no communication. I ran the GUI as written in...

0693W00000Nrtw8QAB.png 0693W00000NrtvoQAB.png
kchan.1 by Associate
  • 1593 Views
  • 2 replies
  • 0 kudos

L6470 Wrong final position with "Goto" command

I have an issue with the "Goto" command of the L6470 driver.Sometimes (rarely) I send a "Goto" command to the driver with an absolute target positon, and the driver goes a few steps (1 to 3) further.The driver is set to work in 1/128 steps.After each...

Manu42 by Associate
  • 2044 Views
  • 3 replies
  • 0 kudos

marking LDK220U50R

Hi, we purchased LDK220U50R and received devices with a marking of: 50306.We didn't find any documentation which explains this marking. Did e received the right part number - please tell us, which marking has to be at LDK220U50R. Thank you

MMP by Associate
  • 1357 Views
  • 1 replies
  • 0 kudos

STPM34 - PH1 Active Energy register(Address 54)

Please advise on the below issue in STPM32 Active Energy Register.Project details -Single Phase Smart Meter. Input voltage - 240VAC and Current - 60A max.Interface - Wifi.Issue - PH1 Active Energy register(Address 54) of STPM34 is overflow once the E...

APK.1 by Associate II
  • 1891 Views
  • 3 replies
  • 0 kudos

L6470 SPI operation

I am confused with the SPI operation particularly the raising CS after each byte (which isn't shown in the data sheet figures). I can get the motor to work, but as an example this is what I have to do to send a simple move command. The data is (in he...