Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Tantalum filter caps for LD1086?

The datasheet for the LD1086 specifies that I should use a 10 uF capacitor to filter the input/output of the device. The datasheet schematic for a typical application shows polarized filter caps. But the datasheet doesn't specify what type of capacit...

Viper 22L

Hi, I need to know whether do you use Viper 22L component? Please respond......

Resolved! STPMIC1 and ST-Link

Hello,Since I'm trying to design a relatively simple and mainly small STM32MP157FAD1 board (MPU, DDR3L, eMMC, WiFi+BT, microphone, speaker and display), something like a wearable motherboard, I'd like to ask if it would be possible to power the whole...

filip1785 by Associate II
  • 3567 Views
  • 6 replies
  • 5 kudos

Date Code for LM2903PT

We have received a part from ST Microelectronics. Kindly provide us with the date code and lot code information for the below part number. I have attached images of the received part for your reference.   

Arumugasiva_0-1691988528177.png

Resolved! Spv1050 battery charging issue

    I have made a custom pcb of STEVAL-ISV019V1  circuit. In that ,we need to charge 3.7v lithium ion battery via USB supply and solar panel. When I connect USB supply or panel voltage as input voltage  the complete input voltage is coming in the bat...

SP1050

Hello,We are using the SPV1050 charger for our device, and we are planning to certify our device with FCC standards, so can you please advise some recommendations on the PCB design to fit the FCC requirements?   Also, someone recommend me to use a se...

Resolved! LED2000 shorts itself when attempting to use the DIM pin

Today I received several of my LED2000DR based LED boards. Everything worked flawlessly when using the chip as a plain LED driver. However, after trying to feed a PWM signal into the DIM pin the dimming worked for about a second but then the board we...

dimin by Associate II
  • 6044 Views
  • 6 replies
  • 0 kudos

Negative Triac supply

Hi,  I have a requirement to drive a Triac from the MCU powered by a DC/DC converter. The AC supply is typ 24 VAC @ Rc terminal with respect to C terminal. The Triac is to be driven as attached. The MCU GND should always regulated at Rc - 3V3. The MC...