Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Searching for spice simulation model

Hello, I'm currently in need of a SPICE simulation model for the USB PD controller TPS65987DDHRSHR. Would it be possible for you to provide me with this model? Your assistance would be greatly appreciated. Thank you.

nesrine12 by Associate III
  • 928 Views
  • 1 replies
  • 0 kudos

素子のひずみについて

・VNH7040AYTR の耐プリント板曲げ性の耐久力をご教授下さい。社内で生産した製品にて2,000~3,000μSTのひずみが確認されました。良品としての使用権を検討したいため、上記の素子のどこまでのひずみが耐えられるのかご教授下さい。

Ushigeki by Associate
  • 838 Views
  • 0 replies
  • 0 kudos

Resolved! STSW-GMBL02V1 cannot connect

Hi Team.I'm trying to connect STEVAL-GMBL02V1 board with STSW-GMBL02V1 control application.The cursor icon becomes a standby animation, but I cannot connect.I connected using the following steps:supply 8V of power to the STEVAL-GMBL02V1 board.connect...

Kenji1_0-1703227174648.png
Kenji1 by Senior
  • 3143 Views
  • 3 replies
  • 0 kudos

Resolved! SPV1050 charge current

For the SPV1050, what is the charge current to the battery? Can I set the current?Also, I would like to verify that when there is no voltage input to the SPV1050 that the two LDOs are off or not operating.

vinsongo by Associate
  • 2095 Views
  • 3 replies
  • 0 kudos

Resolved! IMDS data

Hello support team,our customer HELAG ELECTRONIC GMBH, IMDS ID: 28796, needs the IMDS data for below product: VNN1NV04PTR-E, Rutronik article number: ICIFP45227.Thank you. Ileana Keges

IKege.1 by Associate
  • 2658 Views
  • 3 replies
  • 1 kudos

Resolved! Inquiry about AQP package (QFN-8) among TS33 series products.

Hello.Three product packages are identified in the TS33's datasheet.Among these, the QFN-8 package has 5 NC pins. Is it okay to connect them to VIN or VOUT or GND?I couldn't find a additional explanation for the NC pin, so please check there is anyth...

LSung.1 by Associate III
  • 2583 Views
  • 4 replies
  • 0 kudos

Resolved! TS4061AILT-1.225 device marking

Please advise where I can find the device marking for TS4061AILT-1.225. I was expecting to find it in the datasheet but it doesn't appear to be in there. Maybe a more general question would be how does ST disseminate such information if not in the da...

Resolved! STPM801 : Oring function

Hello,I've developed a PCB utilizing the STPM801 driver and am interested in deactivating its Oring feature.The device I'm working on is battery-powered and operates two BLDC motors. There's a specific requirement to maintain functionality when the m...

L6482 clarification

Hello,I was considering using the L6482 IC in one of my projects, but i need a clarification.What does "AC" mean in the "Full bridge output voltage" absolute maximum specification? (More info in the following screenshot)  

Tensione_L6482.png