Resolved! SPV1050 charge current
For the SPV1050, what is the charge current to the battery? Can I set the current?Also, I would like to verify that when there is no voltage input to the SPV1050 that the two LDOs are off or not operating.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
For the SPV1050, what is the charge current to the battery? Can I set the current?Also, I would like to verify that when there is no voltage input to the SPV1050 that the two LDOs are off or not operating.
Hello support team,our customer HELAG ELECTRONIC GMBH, IMDS ID: 28796, needs the IMDS data for below product: VNN1NV04PTR-E, Rutronik article number: ICIFP45227.Thank you. Ileana Keges
Hello.Three product packages are identified in the TS33's datasheet.Among these, the QFN-8 package has 5 NC pins. Is it okay to connect them to VIN or VOUT or GND?I couldn't find a additional explanation for the NC pin, so please check there is anyth...
Please advise where I can find the device marking for TS4061AILT-1.225. I was expecting to find it in the datasheet but it doesn't appear to be in there. Maybe a more general question would be how does ST disseminate such information if not in the da...
Hello ST Community,I am currently working on a project that involves the use of 2 LIR2450 Li-ion batteries. For the battery charging aspect, I am seeking recommendations for a suitable Power Management Integrated Circuit (PMIC) charger from ST.Specif...
Hello,I've developed a PCB utilizing the STPM801 driver and am interested in deactivating its Oring feature.The device I'm working on is battery-powered and operates two BLDC motors. There's a specific requirement to maintain functionality when the m...
Hello,I was considering using the L6482 IC in one of my projects, but i need a clarification.What does "AC" mean in the "Full bridge output voltage" absolute maximum specification? (More info in the following screenshot)
Hello, I am searching for transistor particularly MOSFETs SCTW70N120G2V spice model. Where can I find it?Thanks
Hello, I am working on BLDC motor driver. I am use STM32G431 as control unit with Motor Control Workbench and DRV8323RH gate driver. I have problem with getting the motor to spin, as soon i I start it, i am getting under voltage error. And see some o...
hiI made a board with stm32l431 and L9963E.The voltage, current and temperature values have been read successfully.In addition, it was confirmed that it operates with settings such as UT, OT, OV, and UV.However, the Fault-L pin does not change to hig...