Power management

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! how STLD40D Driver work?

Hi everyoneI'm going to use STLD40D Driver IC for my TFT LCD. For driving LCD backlight, I'v chosen this Driver from ST. But I can't figure out the function theory of this driver. could you please explain for me the STLD40D function theory and how to...

MSm by Associate II
  • 833 Views
  • 4 replies
  • 0 kudos

Resolved! LED1642GW - Intermittent Illumination

ContextI'm working on building an LED Cube for no other reason but my own self learning. My intention is to use 12 LED1642W to support a 8x8 grid of 3 channel RGB LEDs, with a 13th LED1642W to multiplex the cube's layers. As a minimum viable model, I...

0693W00000Lve3cQAB.jpg
GKerwood by Associate II
  • 1087 Views
  • 9 replies
  • 0 kudos

Resolved! Which IC has "HVLED01A" marking code?

Hi, I have an IC in hand which is written "HVLED01A" on it and I want to know its product number.I wonder is that same as "HVLED001A" product number or it is different IC? Thank you in advance.

MFath.2 by Associate
  • 429 Views
  • 2 replies
  • 0 kudos

Resolved! LED1642GW - Endianness of Configuration Register?

Hello,I would grateful for some clarity on the expected bit order when writing to the configuration register of the LED1642GW.Whilst it is clearly documented that CFG-0 is the LSB, and CFG-15 is the MSB of the serialised word, it is not clear to me w...

GKerwood by Associate II
  • 362 Views
  • 2 replies
  • 0 kudos

Resolved! LED1642GW - No data output on SDO

I have a project whereby I intend to cascade 13 LED1642GWPTRs, in order to control a number of RGB LEDs.As an "in-progress-check", I have currently placed only two LED1642GWs, each as the schematic below, with SDO of the first chip connected to SDI o...

0693W00000KdLjAQAV.jpg
GKerwood by Associate II
  • 439 Views
  • 3 replies
  • 0 kudos

Resolved! LED7708 flickering/flashing issue

HiWe observe sudden changes and flickering especially at low level luminosity.attached oscilloscope capture_1 is taken at one of green LED channels. During the dimming cycle, the ghost pattern causes momentary flashes in LED brightness.again oscillos...

b_1 by Associate
  • 541 Views
  • 1 replies
  • 0 kudos

LED1642GW LED's flicker during brightness changes.

Testing the LED1642GW using the X-NUCLEO-LED16A1 expansion board. I appear to have the communication working using the digital keys for LE on a GPIO output and a SPI interface. I can read and write the configuration register and write brightness valu...

DKeny.1 by Associate
  • 322 Views
  • 2 replies
  • 0 kudos