Hi, We are using Laser TOF Sensor (VL53L1CXVOFY/1) in one of our products.Can we use AVDD=1.8V power supply? Even though AVDD = 2.8V, it looks like IOs will work on 1.8V.
Hi Mike,Laser TOF Sensor (VL53L1CXVOFY/1) power supply?If we connect AVDD (Pin 11) and AVDDVCSEL (Pin 1) to 2.8V, Are the IOs still operate on 1.8V mode as given in Datasheet page number 23, Table 14.>The default driver mode is 1V8.>2V8 mode is progr...
Hi Peter,Thank you for your quick response...Lets take a simple example. Lets take an LED and Anode of LED is connected to 3.3v supply and cathode of LED connected to one of the outputs of LED driver RGB[1:8], lets say R1. To make the LED ON and OFF,...
Hi Peter,Thank you for the quick reply.Can we make them (RGB[1:8]) independently Low (how many volts?) and High(how many volts?) for supply VDD=3.3VIn other words what is the logic levels of these outputs? How to control these Logic levels independen...
Hi Peter,Thank you for the Reply. Actually we don't want to inactive all outputs. We want to control R[1:8], G[1:8] and B[1:8] outputs independently.Can we control these Outputs independently low or high (particular segment LED on/off). If so how?Reg...