User Activity

ContextI'm working on building an LED Cube for no other reason but my own self learning. My intention is to use 12 LED1642W to support a 8x8 grid of 3 channel RGB LEDs, with a 13th LED1642W to multiplex the cube's layers. As a minimum viable model, I...
Hello,I would grateful for some clarity on the expected bit order when writing to the configuration register of the LED1642GW.Whilst it is clearly documented that CFG-0 is the LSB, and CFG-15 is the MSB of the serialised word, it is not clear to me w...
I have a project whereby I intend to cascade 13 LED1642GWPTRs, in order to control a number of RGB LEDs.As an "in-progress-check", I have currently placed only two LED1642GWs, each as the schematic below, with SDO of the first chip connected to SDI o...