User Activity

Hello everyone,I'm developing embedded firmware for stm32mp135f-dk board using Yocto/Bitbake (Kirkstone) with meta-st-stm32mp layer. My question is related to SD card partitions, so please find my flash layout .tsv file below:#OptIdNameTypeIPOffsetBi...
Hello,I am using Yocto (Kirkstone) to develop linux for my embedded linux device, which is stm32mp135f-dk board. In Yocto build system one can set the IMAGE_ROOTFS_SIZE variable, which (along with IMAGE_ROOTFS_EXTRA_SPACE and IMAGE_OVERHEAD_FACTOR va...
Hello,I am working with STM32MP135F-DK and Yocto (Kirkstone), using poky, meta-openembedded, meta-st-stm32mp layers. I am creating my custom image for the board. I want to implement OTA to my board and I have chosen swupdate package to achive that. I...
Hello,we are developing IoT device for which we are planning to use STM32MP135D MPU placed on our custom SoM.To do test before SoM is ready, I have obtained a STM32MP135F-DK. There are some concerns about the 'factory programming' of such device.With...
Hi all,I would like to design a device with the following features:Dual Gigabit ethernet,Encrypted communication: SNMPv3, HTTPS, SMTPS.I am looking for a SoC that makes it possible to achieve this functionality. After doing some research, I have foun...