STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART 4 logging while connected with st link.Also what does this means : LD Linker > Libraries > Small printf?

Hello, There may be another variant of this question available but I am reposting it as I couldn't get any success so far redirecting prinf messages to uart4 and viewing them on serial terminal utility.below are the snapshots which shows I have mappe...

0693W00000NrQ2pQAF.png 0693W00000NrQ2uQAF.png 0693W00000NrQ2zQAF.png
darla14 by Senior
  • 1833 Views
  • 1 replies
  • 0 kudos

Resolved! Debugging methods for FunctionFS Usb gadget in STM32MP1: HDMI-USB C PA10 pin conflict

Hi,I am working on a functionFS usb gadget based on gmidi. Following the gadget_configfs.rst and using stm32_usbotg_eth_config.sh as starting point was straight forward. After writing the shell script and modifying my device tree configuration to sup...

KChar.1 by Senior
  • 12664 Views
  • 27 replies
  • 0 kudos

OpenSTLinux Testing

We are using OpenSTLinux as base distro for configuring and developing product on a custom STM32MP1 based embedded board. We plan to develop some testing and validation plans for the same. Just wanted to understand what sort of testing is carried out...

NPal.2 by Senior
  • 1970 Views
  • 2 replies
  • 0 kudos

Resolved! What is the correct Linux pin control configuration for ANA0 and ANA1 on TFBGA361?

I have a design based on the STM32MP157C (technically the Octavo SiP) which simulatenously uses PA0, PA1, ANA0, and ANA1. While measuring analog signals on the device, I'm noticing that the CPU is biasing the ANA0 and ANA1 signals -- based on a measu...

MWalk.3 by Associate II
  • 2671 Views
  • 3 replies
  • 1 kudos

stm32mp1 simple frame buffer

i have following yocto build configurationBuild Configuration:BB_VERSION          = "1.42.0"BUILD_SYS           = "x86_64-linux"NATIVELSBSTRING     = "universal"TARGET_SYS          = "arm-openstlinux_weston-linux-gnueabi"DISTRO              = "openst...

Ara.1 by Senior
  • 6710 Views
  • 6 replies
  • 0 kudos