User Activity

Hello,I would like to enable battery/capacitor charging from the VBAT pin on an STM32MP1 and also change the charging resistor.That would be VBE and VBRS of PWR_CR3.What would be the proper way to enable/disable the charging together with the resisto...
Hello!I see many having similar issues, but I have have yet to find a solution to the reason my boot is not happening.ATF: v2.2-stm32mp-r2.1U-Boot: 2021.01Linux: v4.19-stm32mp-r3.3Works just fineATF: v2.2-stm32mp-r2.1U-Boot: 2021.01 (Edit: and v2020....
I am trying to boot U-boot as SSBL on a simple board with an eMMC flash.I flash the partitions using the embedded DFU ROMboot with STM32CubeProgrammer using the following Flash Layout#Opt   Id Name   Type   IP Offset Binary-  0x01   fsbl1-boot Binary...