STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32mp157 Ethernet problem

An urgent problem occurred in stm32mp157. I used ksz9031 network chip, but it could not be used. The LOG is as follows,[  18.996823] Micrel KSZ9031 Gigabit PHY stmmac-0:00: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=stmmac-0:0...

Yli.8 by Associate II
  • 9591 Views
  • 8 replies
  • 0 kudos

Make device appear as mass storage device

I have a STM32MP157f-dk2 board, the USB OTG port is configured by default to appear as network ethernet adapter when plugged into the PC. I would like to configure the USB OTG port to appear as a mass storage device when plugged into the PC. I am new...

yhu by Associate
  • 1282 Views
  • 1 replies
  • 0 kudos

eMMC flash without STM32CubeProgrammer

Hello everyone,we have a custom board with STM32MP157F. The board is equipped with SD and eMMC. We do not have USB on endproduct. Our plan flashing eMMC is as follows: 1. create yocto image for eMMC 2. create SD image 3. generate SD raw image with th...

arslan by Associate II
  • 1965 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.