STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP135 NO BACKLIGHT

Hi Everyone,I have problem with custom carrier and dts. I am using MP135 SoM from PHYTEC and when I add panel backlight property to the panel node, there is no pwm output, but when I comment out this feature from the panel node, the panel backlight w...

batuhanky by Associate III
  • 1281 Views
  • 0 replies
  • 0 kudos

PWM backlight not working.

Can you please check my device tree configuration?Backlight as a GPIO is working correctly, but when i try to use it as pwm, the pin line is always fixed to low.Inside my .dts:This is my panel definition:panel { compatible = "newkoro,display","simp...

Lmoio.1 by Senior
  • 9415 Views
  • 10 replies
  • 0 kudos

stpmic1-regulator warnings

Hey there,I have a custom stm32mp153c based board. I adapted bootloaders/optee/kernel from scarthgap branch of meta-st-stm32mp and have everything booting (tf-a 2.8, u-boot 2022.10, optee 3.19, kernel 6.1.28). The only remaining warnings I have are t...

UVV by Associate III
  • 1953 Views
  • 3 replies
  • 0 kudos

SAI in the linux kernel source code, how the two submodules can be received at the same time.

linux内核源码当中的SAI,两个子模块如何同时进行接收,一般正点的sda用于发送,SDB用于接收Translated to Englishlinux kernel source code among the SAI, how the two submodules at the same time to receive, the general positive point of the sda is used to send, SDB is used to receive

Poppy by Associate
  • 860 Views
  • 0 replies
  • 0 kudos