STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PHYTEC STM32MP135 LCD PANEL DTS

Hello everyone,I am using the STM32MP135 SoM from PHYTEC, and I’m creating a custom device tree source (DTS) file tailored to our carrier board. I’m having trouble controlling the backlight PWM signal. I’m unable to enable the PWM and enable signal a...

image_2024-11-05_005132081.png image_2024-11-05_005307530.png image_2024-11-05_005326551.png
batuhanky by Associate III
  • 2131 Views
  • 3 replies
  • 1 kudos

STM32MP135 NO BACKLIGHT

Hi Everyone,I have problem with custom carrier and dts. I am using MP135 SoM from PHYTEC and when I add panel backlight property to the panel node, there is no pwm output, but when I comment out this feature from the panel node, the panel backlight w...

batuhanky by Associate III
  • 1241 Views
  • 0 replies
  • 0 kudos

PWM backlight not working.

Can you please check my device tree configuration?Backlight as a GPIO is working correctly, but when i try to use it as pwm, the pin line is always fixed to low.Inside my .dts:This is my panel definition:panel { compatible = "newkoro,display","simp...

Lmoio.1 by Senior
  • 8999 Views
  • 10 replies
  • 0 kudos

stpmic1-regulator warnings

Hey there,I have a custom stm32mp153c based board. I adapted bootloaders/optee/kernel from scarthgap branch of meta-st-stm32mp and have everything booting (tf-a 2.8, u-boot 2022.10, optee 3.19, kernel 6.1.28). The only remaining warnings I have are t...

UVV by Associate III
  • 1840 Views
  • 3 replies
  • 0 kudos