Solved
How to make STM32MP151 successfully run LINUXPTP
- 9 replies
- 5206 views
STM32MP151 is a PTP slave clock, and the master clock is correctly determined and configured. In the same network, multicast, E2E, and one-step configuration modes are used. Run ptp4l,Output prompt: "Received SYNC without timestamp". the actual SYNC message of the main clock has a hardware timestamp.
Other relevant information can be found in the info1. log file.
STM32MP151 is the PTP slave clock IP: 192.168.1.251, the PTP master clock IP: 192.168.1.3, Captured data packet shows that the master clock has a timestamp, and the slave clock DELAY_REQ has no timestamp.
翻译
搜索
复制