STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Xlib: I can not connect to the X server

Hi!I'm in search of a better GUI programming path :) Now trying Xlib.Here is a simple program from the Internet#include <stdio.h> #include <stdlib.h> #include <string.h> #include <errno.h> #include <X11/Xlib.h> extern int errno; int main( void ) {   ...

AShva.1 by Associate II
  • 1992 Views
  • 2 replies
  • 0 kudos

gtk_window_move does not work :(

Hi!Simple program on board STM32MP157C-DK2#include <gtk/gtk.h>gint width = 400;gint height = 200;gint X = 20; gint Y = 20;gint x; gint y;GtkWidget *window;int main (int argc, char *argv[]){   gtk_init(&argc, &argv);   window = gtk_window_new(GTK_WIND...

AShva.1 by Associate II
  • 2581 Views
  • 2 replies
  • 0 kudos

create_emmc_from_flashlayout.sh

With the Distribution Package for STM32MP1 I created my own machine (STM32MP151A) and I was able to generate a the flashlayout for both sdcard and emmc.I don't see any script to create the image for emmc, like `create_sdcard_from_flashlayout.sh`.Is t...

Mark81 by Associate III
  • 2289 Views
  • 2 replies
  • 0 kudos

How to build a minimal OpenSTLinux SD image with all drivers/hardware support for the DK2 Discovery board ?

I am confused by the different packages ,Starter, Distribution and Developer.Which one do I need to install/setup/build to have as the end result a "minimal" cli/shell based SD card image with support for all hardware on the DK2 board ? a "clean" ro...

mfny by Associate III
  • 2245 Views
  • 2 replies
  • 0 kudos