STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unsuccessfully Adding an external out-of-tree Linux kernel module with Distribution_Package

Following https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Distribution_Package4 Adding an external out-of-tree Linux kernel moduleWhen doing this step, error occurs.PC $> devtool build mymodule...WARNING: /home/tim/STM32MP15-Ecosystem...

tpeng.1 by Associate III
  • 1847 Views
  • 1 replies
  • 0 kudos

在我试用stm32_rpmsg_sdb驱动测试大数�?�传输时,�?�到数�?�传输错误的问题

CM4:基于官方给出的例�?,我去掉通过IO�?�数�?�采样​,采用填充固定数�?�进入缓冲区的方法,在传递到DDR的相应缓冲区中。A7:基于官方的测试例�?,�?写入文件,直接将接收到的数�?�显示到频幕上。​我�?�现,在多次数�?�传输�?�,Linux应用程�?读�?�​的DDR数�?�出现错误,这些数�?�以64字节为�?��?。如下图所示,我填充的时0x1f,但是缓冲区中出现了0x1c和0x16,他们都是之�?写入的数�?�。​请问这个问题�?�能是怎样造�?的。​​​​

0693W000000UwVRQA0.png
Yji.1 by Associate II
  • 4355 Views
  • 9 replies
  • 0 kudos

Use stm32mpu weston image with OP-tee.

Hi,I try use optee with weston image and I find that:Once the machine is defined with MACHINE_FEATURES += "optee" and the distro is set with DISTRO_FEATURES_append = " optee ", building the OpenSTLinux distribution will provide all necessary binaries...

Adrian1 by Associate III
  • 2450 Views
  • 2 replies
  • 0 kudos

Resolved! Trouble building meta-st-stm32mpu-app-logicanalyzer ("backend.c:49:10: fatal error: gtk/gtk.h: No such file or directory")

I need assistance building the https://github.com/STMicroelectronics/meta-st-stm32mpu-app-logicanalyser project. I have the Distribution-Package building successfully, but when I follow the instructions for the example meta layer, I get the following...

JCant.1 by Associate III
  • 4709 Views
  • 11 replies
  • 0 kudos

Stm32mp157, CubeMX and Touchgfx

I can select stm32mp157 in cubemx, but I can't configure peripherals.​will it possible in future? When?​C​an I make projects with TouchGFX for mp157 with cube MX in future​ I want to use this module http://www.myirtech.com/list.asp?id=624

EEuge by Senior
  • 2859 Views
  • 4 replies
  • 0 kudos