User Activity

board: stm32mp157a-dk1device-tree:pinctrl{ usart2_pins_b: usart2-0 { pins1 { pinmux = <STM32_PINMUX('F', 5, AF7)>; /* USART2_TX */ bias-disable; drive-push-pull; slew-rate = <0>; }; pins2 { pinmux = <STM32_PINMUX('F', 4, AF7)>; /* USA...
CM4:基于官方给出的例�?,我去掉通过IO�?�数�?�采样​,采用填充固定数�?�进入缓冲区的方法,在传递到DDR的相应缓冲区中。A7:基于官方的测试例�?,�?写入文件,直接将接收到的数�?�显示到频幕上。​我�?�现,在多次数�?�传输�?�,Linux应用程�?读�?�​的DDR数�?�出现错误,这些数�?�以64字节为�?��?。如下图所示,我填充的时0x1f,但是缓冲区中出现了0x1c和0x16,他们都是之�?写入的数�?�。​请问这个问题�?�能是怎样造�?的。​​​​