Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.
Hi,i created a DT in Cubemx and now everythings works fine, with the exception of the CAN Bus.Here are the Snippets of the Device in DT:/// Clocks section CLK_FDCAN_PLL4R in the Clocks Section /// &m_can1{ pinctrl-names = "default", "sleep"; pinctr...
Which setting do i need? right now i try to build u-boot as debian package with follwoing settings:dpkg-buildpackage -a armAt the begining of the compilation i get following error:dpkg-architecture: warning: specified GNU system type arm-linux-gnu do...
Hi All.I develop M4 Core firmware using a custom board based on STM32MP151C.There is no problem with SPI communication without using DMA. However, when DMA is used, waveforms do not occur the pins or only the NSS pins react, resulting in waveforms.I...
Hi,I have created a layer with my custom distro config and altered the conf/local.conf to point to this new distro. So far so good, everything worked as expected. Now comming back and I want to resource the environment with source ./layers/meta-st...
####Error messages are below..ERROR: gstreamer1.0-plugins-bad-1.14.4-r0 do_compile: oe_runmake failedERROR: gstreamer1.0-plugins-bad-1.14.4-r0 do_compile: Function failed: do_compile (log file is located at /home/kheng_sw/work/STM32MP1/Distribution-P...
I installed st-example-image-x11.Matchbox windows manager started on foto.And ! have 2 problem. Till.1st problem.I can not change the orientation of the matchbox panel. I changed the lines in the /usr/bin/matchbox-session file: matchbox-panel --orien...
Hi Guys,I’m having an issue connecting a touch screen to stm32mp157a-dk2. My Qt application crashes with a “Segmentation Fault�? when I touch the screen multiple times in quick succession.Has anyone else reported this problem before?Here is my setup:...
Hi, i want to use node.js on STM32MP157C-DK2. I found this post https://community.st.com/s/question/0D50X0000B0xovG/installing-nodejs-on-the-stm32mp1 , but I dont want to rebuild the imageIs there a way to install node.js without rebuilding the image...
Hi. I have generated a full device tree for the EV1 to add I2C5 pins PA11/PA12 for external connector hookup to some of my I2C widgets using STM32CubeMX. I've place the generated .dts file from the kernel/ folder into <linux-source>/arch/arm/boot/dts...