User Activity

Hi,i currently trying to interact via shellscript and stm32cubeprog cli with my stm32mp157 board.I can run and load tfa and than uboot. But when i want to read otp, my operations get stuck.What is the correct call for this?In my Script is use the fol...
Hi,we are currently testing our FDCAN on our STM32MP157F Device. We get some Messages that there ist an access violation. We see that is caused by the M_RAF interrupt. Are there any hints to get rid off these messages and errors? We tried different s...
Hi, we are currently bring up our custom STM32MP157 Board. We get in any constellation a "DDR addr bus test: can't access memory @ 0xc000004"We think that our crystal is correctly running at 24 Mhz because we connecting over USB to the Board. Also th...
Hi,for our testing i want to activate the fullspeed OTG on the Pins PA11,PA12. VBUS_OTG is not routet out the Chip on the DK2. Is it possbile to use the FS phy on PA11/PA12 on the DK2 board?Best regards,Niklas
Hi,we are currently evaluate the STM32MP for a project and we want to ensure that we can handle all errataissues that concern our usage scenario.In Errata are the points: 2.6.1 to 2.6.4 that discribe DMAMUX issues. At this point my question is:Does L...