User Activity

Hi ST.I set the clock in the dts file as below.&rcc { st,hsi-cal; st,csi-cal; st,cal-sec = <60>; st,clksrc = < CLK_MPU_PLL1P CLK_AXI_PLL2P CLK_MCU_PLL3P CLK_PLL12_HSE CLK_PLL3_HSE CLK_PLL4_HSE CLK_RTC_LSE CLK_MCO1_DISABLED CLK_MCO2_DISABLED >; st,clk...
Hi STI have a question when setting the ADC Clock on the M4 Core side.The STM32MP151C datasheet states that the ADC Clock can be set up to 36Mhz.When the AHB clock is 200Mhz, what clock will it work with if I set "ADC ClockPrescaler" to "ADC_CLOCK_SY...
Hi STI enabled DISTRO_FEATURES_append = "tpm2" in the file ".../layers/meta-st/meta-st-openstlinux/conf/distro/include/openstlinux.inc" as described in the ST Wiki.When building with "st-image-weston" I get the following error message:ERROR: Nothing ...
Hi AllWhen building "Eco system V2.1.0" distribution of Custom Board based on STM32MP151C chip, there is a problem that devicetree symbolic link is not created.Symbolic link of custom board devicetree is not created in "tmp-glibc/work-shared/stm32mp1...
Hi All​​If you create a distribution with RTL8723BU enabled in the Linux kernel and boot, you will see the error message below.[  30.102790] usb 2-1.2: 1f8: ff ff ff ff ff ff ff ff[  30.106213] usb 2-1.2: RTL8723BU rev E (SMIC) 1T1R, TX queues 3, WiF...