STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet not working in u-boot: "Could not get PHY for ethernet@5800a000: addr 0 phy_connect() failed"

hi,I am working with a custom board based on the STM32MP157C. I use a lan9303 chip which is acting as a switch for ethernet. In the linux kernel, there are no problems with the ethernet but I can't get it to work in u-boot. Even when I use the same D...

sgtl5000 codec dsi i2c

Hi All,i am using stm32mp1 with i2c on sgtl5000 codec and control lines are over carrier i2si am getting kernel soc sgtl5000.c error sgtl5000 0-000a: Error reading chip id -6<STM32_PINMUX('A', 15, AF5)>; /* I2S1_WS */<STM32_PINMUX('Z', 0, AF5)>, /* I...

Ara.1 by Senior
  • 18041 Views
  • 52 replies
  • 0 kudos

Resolved! Uboot not executing board_init function?

I'm using the bootlin buildroot branch: st/2021.02.I want to run a certain function on init of the Uboot (board_init function), like the ones used for the DK1 and DK2. My problem is that the function doesn't seem to be called. I have tried to debug t...

jhi by Senior
  • 1839 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP157A-DK1 remoteproc to M4 failed

Hello, i'm trying to use M4 kernel from A7 kernel worked under linux.I've started with openSTlinux distro and it works well (i can upload firmware to M4 using rproc), but for some reasons i need to make a very small distro (less than 16 mb). For this...

OMORO.1 by Associate II
  • 4188 Views
  • 6 replies
  • 0 kudos

Resolved! stm32mp157c quad spi flash driver

Hi,I'm working the stm32mp157c som and trying to boot external quad spi flash (cypress S25HL512T). I added this to dts. &qspi {   pinctrl-names = "default", "sleep"; pinctrl-0 = <&quadspi_pins_mx>; pinctrl-1 = <&quadspi_sleep_pins_mx>; status = "...

aliMesut by Associate III
  • 4020 Views
  • 4 replies
  • 0 kudos

Resolved! In the STM32MP157 I am trying to program an interrupt every 100 us using timer 14. It looks like the code generated is correct, but the result is not correct. It looks like the DiV4 has no effect. The timing is the same as no divide.

Looking at the clock in the MX Device Configuration Tool it says 204 to APB1 Timer Clocks (MHz).To get to 10000 Hz I have to divide 204 MHz by 20400. Fortunately there are a bunch of ways to do this. But on the first try I tried Prescaler 51Counter ...

KiptonM by Lead
  • 2834 Views
  • 3 replies
  • 0 kudos