Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L7983PU50R

Hello,I am currently developing a device that uses the L7983PU50R as a 5V power source, based on the L7983PU50R - Evaluation board schematic.In the circuit, the 5V output is further used to power an LDO with a 3.3V output and a reference voltage sour...

Can't find STBC15QTR anywhere, it is out of production?

Just finished my design for wireless charging board with the STBC15QTR as charging controller. The chip marked as active production but i can't find the chip on estore.st.com, mouser or digikey. Where can i buy it?I could switch my design to STBC15LJ...

vasimv by Associate
  • 1079 Views
  • 1 replies
  • 1 kudos

STUSB1600 can't work as source

Dear All, Hello everyone, I used STUSB1600 as the type-c dual role type power management. When it works as sink type, it is good. But when it works as source type, it doesn't work. I found VBUS_EN_SRC always keep high. This is my design schematic, co...

Gerald_W_0-1728090554208.png Gerald_W_1-1728090575191.png
Gerald_W by Associate III
  • 4709 Views
  • 12 replies
  • 0 kudos

L6482 behaviour at high speeds

Hello,we want to use L6482 chip to substiture DRV8711 driver we have been using so far. However from our tests the driver does not behave equally as well. We took some oscilloscope screenshots showing that at high speeds the current provided to the m...

Resolved! Current sense on high side driver VNQ9025AJ

Hey,I'm planning to use this high-side driver in a project distribution module, but I'm having trouble fully understanding how the current sensing works.I've looked at the schematic, and I see a combination of two resistors, Rprot and Rsense. Is this...

Captura de tela 2024-10-07 192133.png

Need DPAK MOSFET with high avalanche rating

We've been using the On Semi FDD8453LZ MOSFET (40V, 6.7 ohm, DPAK) in our motor control designs for many years, but this part is now EOL.  We're looking for a suitable DPAK replacement.  One critical parameter is the single pulse avalanche energy, wh...

WiscEng by Associate
  • 808 Views
  • 1 replies
  • 0 kudos

SPV1050 BATT_CHG output

Dears,There is SPV1050 in my circuit. Works without MPPT, boost mode. The problem concerns BATT_CHG state. Documentation says BATT_CHG output reflects DC/DC converter state, i. e. it is active (low) when DC/DC converter works. Simply saying:1. When i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.