User Activity

Hi,I am using LNBH23 and LNBH26 for our LNB control. And I have the following question:1) When I power LNB with 18VDC, I can enable/disable 22KHz properly.2) When I power off LNB, I can't enable 22KHz.Anyone can tell me how to enable 22KHz without LN...
Hi,   I am using L6470 for our stepper motor. Can I use it as motion tracking? Just like: If I change the target position, it will move to it... If not, is there any stepper motor drive from ST that can do it? Thanks, Christie
Hi,I am usinga) L6470 to control Stepper motors. I am using STP-MTR-23079(x). The motor has rated current=2.8A/phase, Resisteance=1.1ohm/phase.b) I am using 24VDC for L6470.c) I am setting KVAL = 14.04% with phase current that is around 3.07A/phase. ...
Hi,Can you tell me if STiD135 is EOL for now?Is there any alternative from ST?Thanks,Christie