Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STWBC86 Refrence 5W design

Hello,Could you please direct me to a complete reference design schematic? The one provided in the datasheet appears incomplete, and many of the forum links on this topic seem to be inactive.Your assistance would be greatly appreciated.

Fritz1 by Associate
  • 986 Views
  • 1 replies
  • 0 kudos

Resolved! STLQ020 reverse protection diode?

I'm working on a low-power design and planning to use a STLQ020. The datasheet doesn't mention the need for a protection diode, nor does it mention that there is one integrated..Is there an integrated protection diode?

CptSlow by Associate
  • 1081 Views
  • 1 replies
  • 0 kudos

L6474 Driver Stalling at 15kHz step frequency

Posted on August 05, 2014 at 00:06Hello,   We're having issues with the L6474PD driver and stalling. I'm testing it with the L6474PD evaluation board powered by 24V. Logic is at 3.3V. Motor runs fine below 15kHz, but right around that frequency it s...

L6474PD

I am working on L6474PD motor Driver.I could figure out that, if the  input is  between 8-48v  it would internally regulate the voltage and supply to the logic circuit of L6474PD , but my question is will the L6474PD independently drive the stepper m...

L78xx datasheet formatting

Through the Characteristics chapter of L78XX DS, the page break is placed incorrectly so, that the conditions - and sometimes also the first row of the table itself - is at the preceding page. Yes, it's formally OK, but is this how ST intends to pres...

waclawekjan_0-1731749085680.png

How to get Equation2 in AN5287

Hi there,I am studying the application note: AN5287. It provides lots of helpful information about SMPS calculation.But I don't understand Equation2.  What is original formular for this?RegardsAlex Chen 

AlexChen2011_0-1731560733895.png

I need the name of this sop8 IC

millenium mps 1000 drum moduleI need the name of the sop8 integrated circuit. The ST logo on it says ua gb145. The 8th leg is +12 volt input. The 7th leg is gnd. The 3rd leg is 2t1 smd push button. The 1st leg is out +12. Can you tell me what this in...

1000132200.jpg
Volkann by Associate II
  • 3107 Views
  • 6 replies
  • 11 kudos

STSPIN958 EN Delay

Have a quick question. What is the delay time from when the EN is pulled high to when the half bridge becomes non Hi-Z? Similar is disable delay time from when the EN is pulled low? I wasn't able to find this information in the data sheet. We will b...

twjudge by Associate
  • 946 Views
  • 1 replies
  • 0 kudos