2023-11-09 10:17 PM - last edited on 2024-06-09 6:37 PM by willzhou
Hello,
Looking through the data sheet for the STWBC86, there doesn't appear to be a way to write to the FTP (Few Times Programmable) memory, nor save individual configuration register values over i2c.
Any register values are only written to RAM and lost upon reboot... No worries, use the FTP memory for the config, but there doesn't appear to be a command in the data sheet to either:
If neither is possible which would be strange, what's the recommended process to program the chip at the factory?
Solved! Go to Solution.
2024-01-24 2:51 AM
Hello,
Sorry for the long delay, I can understand your frustation.
Concerning the FTP programming, you can find the answer in the GUI user manual:
https://www.st.com/en/embedded-software/stsw-wpstudio.html#documentation
You have 2 ways to modify the parameters:
- by changing the register values directly in the GUI : the new value will be applied on-the-fly (note that it is true only for the parameters which appear in black, the ones appearing in red must be modified through NVM writing). The registers will be restored to their default values at next power-off.
- by creating a configuration file (after register modification in the GUI, press "Save TX" command to create your file) and writing the files in the NVM using "Programming" menu of the GUI. This menu can be used to program the latest patch version if needed (default config file and patch file can be found here: https://www.st.com/en/embedded-software/stsw-wbc86fwbpp.html)
For production stage, you can decide to create an unique Header file, using the "Header Generator" menu of the GUI. Then, both Configuration and Patch files can be loaded at once by your production tool (the driver and some instructions are available on Github: stwlc38/README.md).
Let me know if you have more questions.
Regards,
Didier
2023-11-14 7:54 PM
Bump, any one know a way to actually program it into non-volatile memory via i2c?
Strange its completely absent from the data sheet.
2023-11-19 8:17 AM
Bump
2023-12-07 10:34 AM
Bump
2023-12-08 2:23 AM
Hey @AnkhInnovationsLLC I am stuck at the same problem. Were you able to figure out how one could program the FTP of STWBC86? I have obtained the header file from STSW-WPStudio and I was thinking to use that header to program the chip. Any help would be appreciated.
2023-12-08 9:49 PM
Nope, I'm still waiting on this thread for an answer from ST on how to actually do it via i2c.
Without it, I'm not sure you could even go to production with any configuration register changed, because the windows app is most likely looking for a specific USB PID as the USB to I2C bridge.
Pretty annoying no one from ST has replied in > 28 days...
2023-12-11 1:32 AM - edited 2023-12-11 1:32 AM
yeah right? You might also have tried contacting them through Submitting an issue on the website. Did you got any help from them?
2023-12-15 3:59 PM
No answers from ST still on how to actually program the FTP memory on the STWBC86.
It is not in the data sheet.
2024-01-22 10:41 AM
More than 2 months since starting this thread and more than 1 month with an open ticket, got an escalation, then zero responses.
Jesus, ST has terrible support...
2024-01-24 2:51 AM
Hello,
Sorry for the long delay, I can understand your frustation.
Concerning the FTP programming, you can find the answer in the GUI user manual:
https://www.st.com/en/embedded-software/stsw-wpstudio.html#documentation
You have 2 ways to modify the parameters:
- by changing the register values directly in the GUI : the new value will be applied on-the-fly (note that it is true only for the parameters which appear in black, the ones appearing in red must be modified through NVM writing). The registers will be restored to their default values at next power-off.
- by creating a configuration file (after register modification in the GUI, press "Save TX" command to create your file) and writing the files in the NVM using "Programming" menu of the GUI. This menu can be used to program the latest patch version if needed (default config file and patch file can be found here: https://www.st.com/en/embedded-software/stsw-wbc86fwbpp.html)
For production stage, you can decide to create an unique Header file, using the "Header Generator" menu of the GUI. Then, both Configuration and Patch files can be loaded at once by your production tool (the driver and some instructions are available on Github: stwlc38/README.md).
Let me know if you have more questions.
Regards,
Didier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.