2024-06-06 9:51 PM
Hi,
we are using L9960 H-Bridge -L9960 for automotive application.
Here are the inputs to consider using L9960.
| Parameters | Min | Typical | Max | Remarks |
| Input Voltage (UBAT) | 8. V | 13.5 V | 18. V | L9960 device will supports 4.5V > < 28V |
| Output Voltage (Out) | 7.4 V | 12.3 V | 15.75 V | Output voltage almost same due to FETs switching |
| Input Current (IBAT) | 3. mA | 4. mA | 5. mA | Device current consumption for normal operation |
| Output Load Current (ILOAD) | 2. A | 3. A | 5. A | L9960 device will supports 1A > ILOAD < 15A |
Could you please help me with power dissipation calculation of this IC. I am aware of this application note an4867-l9960-l9960t-automotive-integrated-hbridges-stmicroelectronics.pdf .
But can i get any worksheet for the same for doing power dissipation calculation?
2024-06-07 11:35 AM
Hi Amrutha
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Kind Regards
Joe
STMicro Support
2024-06-08 10:46 PM
Sure, Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.