Resolved! STEF033AJR usage
From Figure 12.STEF033 cannot be used for the case Ilim=1A?Rlimit is valid when the value is more than 120 ohm?
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
From Figure 12.STEF033 cannot be used for the case Ilim=1A?Rlimit is valid when the value is more than 120 ohm?
Hi everyone, I'm working on a prototype, which is using a PM8805 to classify connected PoE types. However we are running into an issue, where neither T0, T1 or T2 are giving us any signals (giving always 1 on their open drain signals, making .the LED...
Hello,We are currently looking ahead at future options for stepper-motor control and are interested in ST’s longer-term direction beyond L6470 and powerSTEP01.For our application, sensorless detection of stall, obstruction/collision, and increased fr...
Hi ST team,We are going to design variable programable power supply based on PFC + half bridge PWM controller (with fixed transformer turns ratio). Below is the requirementFor Model 1 Vout (Half bridge converter): 3V-63V/5A (180W maximum with auto ra...
Hello,In the STPMIC datasheet, the BSTOUT continous current is specified as being greater than 1.1 A when 3.3 V < VIn < 5.5 V.If the voltage Vin is greater than 4.5 V, does the BSTOUT continous current increase?I assume so, since the inductor's pe...
The Tsample value doesn't reach the published value (between 0.3 and 0.5 s, and from my measurements between 0.3 and 0.35 s) until Vstore reaches the EOC threshold. Before, it is just around 80 ms. Once EOC is reached and when Vstore decreases again ...
Hi ST team,We are going to use L6598D PWM controller (Half bridge topology) followed by PFC IC L4985B for our variable power supply design.We need two models for variable (programable) power supply (Model 1 & Model 2) as below specifications. So, can...
Hi, We are currently using the parts listed below and would like to confirm if they are reflow compatible. We plan to use a paste-in-hole (pin-in-paste) process for these through-hole components during SMT assembly. Could you please advise if the fol...
Hi Engineer, Based on the data sheet, the marking of STH145N8F7-2AG should be "145N8F7 ", but the parts I purchased were with marking of "145N8F7-2". Could you help suggest whether I purchased correct parts? Thanks, Haddy
Hello,I am currently working with the STEVAL-L99615C evaluation kit and the Nucleo G071RB microcontroller board. My goal is to set up a LabVIEW program that can:1. Adjust the output voltages of power supplies to simulate real battery cells.2. Read da...