Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Communication via SPI with L6470 in mode daisy chain

Posted on October 09, 2012 at 10:45Hello I'm trying to communicate with SPI from my application in C with two L6470 configured in daisy chain mode. Sending data but I get no response from the pin DSO of  the first L6470. Someone can tell me the step...

jartigas by Associate II
  • 3024 Views
  • 8 replies
  • 0 kudos

L6561/L6562 MathCad design tool

Posted on October 30, 2014 at 22:06The document AN1089 CONTROL LOOP MODELING OF L6561-BASED TM PFC by Claudio Adragna says: ''As a tool to ease the design of L6561�s E/A compensation networks in TM boost PFC preregulators, the Appendix contains a Ma...

jbright by Associate II
  • 1253 Views
  • 1 replies
  • 0 kudos

L6229Q EN internally connected to DIAG

Posted on October 21, 2014 at 00:52In the datasheet for the L6229Q, section 5.2 states ''Pin EN (Enable) has identical input structure with the exception that the drain of the overcurrent and thermal protection MOSFET is also connected to this pin.'...

jcarlson by Associate
  • 927 Views
  • 1 replies
  • 0 kudos

No working devices issue.

Posted on October 17, 2014 at 05:56 Hello, I see this question in the forum, but no one reply. Can anyone help to feedback how to solve this problem? Because I encountered this issue too. Thanks. ===========================================...

0690X0000060MoWQAU.gif

Motor electrical parameters

Posted on October 24, 2014 at 14:53Hi, I am not entierly sure how to correctly enter my motor parameters, and which effect they have, can anyone check if I am doing this correctly (sensorless operation with cordic startup, no extra features like flu...

Need recommendation for Full Bridge Driver

Posted on October 26, 2014 at 05:55I need a Full Bridge driver IC capable of at least 2.5 Amps at 125 kHz.The L6225 connected in parallel looks good but the highest frequency is only rated to 100 kHzIs there a higher frequency version of this or can...

sales by Associate
  • 656 Views
  • 0 replies
  • 0 kudos

Motor Electrical parameters Rs and Ls

Posted on October 21, 2014 at 02:19Gigi:        I have a question, measured in workbench Motor Electrical parameters Rs and Ls. I see ST data is used RLC meter measurement frequency at 100 Hz, but the motor is running in the PWM 16K frequency, wheth...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.